Solution
Vehicle Crash Test Load Cell Wall
A facility wants to do vehicle crash wall tests. They need to measure the force of the vehicle crash tests, on all axis.

A facility wants to do crash tests on their vehicles. There are multiple tests such as structural testing of the vehicle, developmental tests, and regulatory and compliance tests. They need to measure the force of the vehicle crash tests, on all axis.
Interface’ suggests using multiple 3A400 3-Axis Force Load Cells, and attach it to the back of a cement crash wall. When connected to the BX8-HD44 Interface BlueDAQ Series Data Acquisition System, force result measurements will be recorded and displayed with the customer’s PC or laptop.
The customer was able to measure the force of impact for all of their different vehicle crash testing demonstrations.
BX8-HD44 Interface BlueDAQ Series Data Acquisition System